Hi
My customer is using the BQ34Z100-G1, in the four LED format, led not always on (LED/COMM Configuration Bit 3 is clear)
We are using the datasheet SLUSBZ5 –JANUARY 2015
He would like to set-up the gauge to automatically light up the LED when the capacity hits below 25%.
Therefore he needs to only set alert for lesser than maybe 25% of batt capacity .
I would like to check with you the following:
- Is the RCA mentioned the datasheet, page 40/60 set by the SOC1 and SOCF (found on page 25)? Is this the right place to set the threshold for less than 25% capacity?
- On table 22, there are a list of alerts that are Or-ed together. How do we mask off the alerts that are not needed?
Ivan