Dear Specialists,
My customer is considering UC2853A it's frequency is 25kHz to 50kHz by output synchronization.
According to the application note(U-159), it was recommended 95kHz to 115kHz.
But I think it has a possibility to use from 25kHz to 50kHz because it is far enough from DC.
Could you please advise possibility and any worries with device inside operation?
If it is possible, please tell me the way to make it happen.
(I think that is U-159 of Figure 11. I am happy to give me additional suggestion. )
If it is impossible, please tell me the reason.
Best regards,
Shinichi