Hi,
I´m not very sure if bq25570 can charge Manganese Lithium Coin Batteries (like for example the ML2020).
The charging recommended circuit for this kind of batteries is a 3.1V from Regulator Output (That´s OK for VBAT_OV value), but then you need to limit the current with a series resistor. (See the recommended circuits for charging from this Panasonic Battery). In case of ML2020 you need to limit it to 3mA when battery is at 2.5V and they specify to place a 180 Ohm series resistance between the Reg Output (VSTOR) and the battery itself.
My doubt is that I think that due that the bq25570 charge control is based on voltage values (VBAT_OV), and that you have a series resistor to limit current with the battery, you are always seeing the 3.1V on VSTOR pin, independently of the REAL batt charge status, so you are really not charging OK this kind off batteries, due that the bq25570 will continously enter on Overvoltage detection.
Any Ideas??
Is better to select other chemistry?
Thanks in advance for your ideas.....