Hello.
it is question to TPS2553.
Look at datasheet P4.
PARAMETER tr Rise time, output Min Not data.
ton Turnon time Nin and typ NOt data.
Would there be reference data?
thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello.
it is question to TPS2553.
Look at datasheet P4.
PARAMETER tr Rise time, output Min Not data.
ton Turnon time Nin and typ NOt data.
Would there be reference data?
thank you.
Only the maximum time is useful and guaranteed in the datasheet. If you would like to use or have reference to the typical and minimum data, I can search for that. But this is only reference data and will not be a guarantee. Do you still want to see the other reference data?
Hello.
Eric Wright san.
Thank you very much for your answer.
Yes. I want to see the other reference data.
Thank you.
Please see the following data:
tr Rise time, output, VIN=2.5V, Minimum (data for Mean - 6 x sigma) = 0.59ms
tr Rise time, output, VIN=6.5V, Minimum (data for Mean - 6 x sigma) = 0.95ms
ton Turnon time, EN, Minimum (data for Mean - 6 x sigma) = 1.5ms
Note that these data do not include the guardbands that would normally be reflected in the datasheet numbers.