If the device is shorted for the load, what current does the translate to on the input power pins? I understand this device has short circuit protection and limits the current to 10 Amps. So does that mean 10 Amps will be flowing into the supply input (pin 4,5,6) as well?