Hi All,
We are looking for a li-ion battery charger with power path management that satisfies the following use case scenario.
We have a requirement in which we need to design a standalone battery operated device that can also act as a power bank to a phone.
The following block diagram explains our use case.
Lets assume the USB charging port is DCP(1.5A current) and the phone and battery charger detects it as DCP(Please assume the charging port detection mechanism by phone and charger is taken care of). In this case, the phone will try to draw 1.5A of charging current while there is an efficiency loss due to buck (inside charger) and boost regulator which will limit the current to way less than 1.5A.
Is there any way we can get rid of buck and boost regulator so that the phone can charge at 1.5A? Is there any battery charger that can provide 5V output(same as USB input), while still monitoring its current for power path management?
Please suggest.
Thanks,
Naveen