Hi,
Can we control 400V output with 0 to 8V control input, if yes how in either of these 2 EVMs ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Atul Bhakay,
Thank you for your interest in these products.
Unfortunately the information you have supplied is not sufficient to allow me to provide a useful answer.
What is the input power source? Does the 400V output need to be isolated from the input power source? What is the power level that you require? What level of output current is being drawn when the output is being reduced from 400V? Over what range of voltage does the 400V output need to be controlled? What level of efficiency do you require when the input voltage is reduced?
Best Regards
Joe Leisten
Hi Atul Bhaky,
Assuming that you want to control the output all the way down to 0V and 0A the LLC converter topology is not a good choice. The LLC converter must deliver a minimum current when working into a short circuit. Please see this document for more details of this:
A better suggestion would be to use the phase shifted bridge converter such as LM5046. Colin Gilmor can help you with this part.
Thanks
Joe Leisten