Hello,
I have the docuement SLUA705 about bq500211A chip.
On the page 3, there is a schematic about implementation of the chip.
I think that there is an error on the schematic.
On the component U2 (on the left corner), the '+' symbol is on the pin number 3 and the '-' symbol is on the pin 1.
The datasheet of the component LMV931MG say that the '-' entry is on the pin 3 and the '+' entry is on the pin 1.
Does someone can confirm the source of the mistake? Which signal should be connected on the '-' entry and which signal should be connected on '+' entry.
Regards,
Guillaume