Hi,
We have designed UCC2803MDREP based triple output Flyback regulator. The main output (master) is +5V, 5A, The other two (slave) outputs are +/-15V and 750 mA.
During testing, we observed that we need some minimum load on +5V output in order that there is no load regulation issue at +/-15 V.
At present, this minimum load requirement on +5V rail is 2.7 A to achieve the above condition. We want to keep it bare minimum say 1 A.
Please advise how this can be achieved. Is there any modification to be done to control loop or any other circuit modifications are required?
Thanks,
Makarand Gadgil