HI ,ti power experts.
I plan to use tps61027 in my design. Now I meet a problem how to calculate the inductor parameter
my requirement is :
vin: 2~3v battery
vout : 5v , 50ma.
I try to calculate the paramter according to the formula (4)&(5) in datasheet.
IL=50ma*5/(2*0.8)=156ma
I chose 20% ripple , switch freq is 600K(typical)
L =2*(5-2)/(156ma*0.2*600*5)=64.1UH
I seems that the inductor value is too high. In the datasheet ,typical application inductor is about 6.8uh.
So can you please give some suggestion ?