This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Timer Module Problems



Hi,

I have to generate intervals of some tenth of microseconds Controlling Hardware.

I tried to use the T24 free running timer and it seems that the timer works.

Unfortunately I cant find a pin to get the info 'interval elapsed' out.

There should be a pin TCMP, but I cant find this pin in the function description of the QFN 64 parts (also not at the QFN 40 parts).

There is a odd description how to use a Output pin, they talking about PWM_OUT_ACTION and PWM_OUT and PWM_OUT_DRV. Each of the four PWM16 Counters have such register-bits, but there were far to less Pins??

Ok, I guess that maybe the Pins PWM0 and PWM1 on my UCD3138OL64EVM can be the Pins I searched for, but dont Looks like.

So can anybody clearify that?

How can I set an external Signal after T24CMP1 have found a match? Maybe there is sample code out?

With best regards

Gerhard