Is there an inherent body diode in GaN power FETs? If so, what is the V/I curve for that?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there an inherent body diode in GaN power FETs? If so, what is the V/I curve for that?
3rd quadrant mode refers to when current flows from the source to the drain of a FET. This is in reference to the typical IV curve of FETs that have Vds on the x axis and Ids on the y axis, since the plots that refer to the mode of operation at this point occur in the 3rd quadrant of the graph. Typically for power FETs this current would conduct through the inherent PN junction diode that is present, but the GaN FETs that are in the LMG5200 do not have this structure so the FET 3rd quadrant operation occurs instead.
Since this is a function of the 3 terminal GaN FET device this will occur when you apply a voltage to either FETs in the LMG5200. The bottom FET will conduct in 3rd quadrant mode when you apply a voltage or attempt to source current from PGND to SW and the top FET will conduct in 3rd quadrant mode when you apply a voltage or attempt to source current from SW to Vin.