When using the UCC28070 Excel Applications Design Tool to start a new design, the spreadsheet will not allow me to change the input voltage range. I would like to change the minimum input voltage to approximately 180V, instead of the 85V that was selected as part of the SLUA479 app note design.
Is this a good tool to use to select component values for generic designs? If so, it would be helpful if the user could select his/her own input voltage parameters. When I try to unlock the cells, it requires a password.
Thanks,
Jason