I try to build a buck converter with some basic components and controlled by a DSP 28335.
Actually, the inductor current is not directly measured. It is a voltage signal from a current transducer.
When I set a switching frequency as 8.8Khz, the waveform of the inductor current is OK as shown in the figure below:
However, when I set the switch frequency as 88Khz, the waveform of the inductor current has a high resonant part when the switch is ON and OFF. It is shown below:
I do not know whether this distortion is caused by the circuit design or the transducer. The capacitor and inductor I use are 100uF and 500uH. Is it because of my large cap? Any one can give some advice for trouble shooting?