Looking for some clarification on driving the Va pin (analog) of the ADC128S102 using the LM4120.
The EVM for the ADC, document snau167 shows 1000pF + 0.047uF on the Va pin of the ADC.
(a)
Document snvs049c for the reference, the LM4120, p.11, "Application Hints" states that values above 0.047uF must be tantalum. What are the recommended capacitance values (types, and ESR) to use when using the LM4120 to power Va? Document snau167 shows Va being driven by the LM4120 - is this design recommended?
(b)
Looking at figures 24 or 27 of snvs049c, can a transistor be added to allow increasing the load capacitance of the LM4120?