Dear Members,
I have a problem of TPS62130 broken frequently.
The adopting conditions are
The input voltage is 12V.
The load current is 1.2A.
The switching frequncy is 2.5MHz.
Coil inductance is 2.2uH.
Output capacitance is 22uF ceramic.
Input capacitance is 10uF ceramic.
I have two broken chips that SW pin -GND pin shorted and one chip that non-switched pulse(non HI voltage).
All of these broken chips were suddenly death.
I had tried to investigate the cause of broken as follows,
1. I checked the temperature of the chip top. That is 55 degree Celsius.
2. Output voltage ripple is 10mVpp. Output voltage is 5.5V.
3. The overshoot and undershoot voltage are 1Vp on switching dead time. The pulse width is 5nsec.
How can I get the cause of the broken?
How should I investigate any other item?