This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error of remaining capacity with bq78pl116



I use a fuelgauge 78pl116 configured in 10mWh. my battery is a 82Wh,  after the end of charge, I have in remaining capacity 93Wh. When I low discharge, I have information erroneous after ten seconds, passage of the remaining capacity in more 400Wh yet the datasheet indicates a range of 0 to 325Wh. why Iha ve this error in remaining capacity? the bit 15 of remaining capacity can be at 0 normally. why is the bit 15 of remaining capacity go to 1?