Hi,
I'm looking for a power MOSFET used in brushless DC motor application.
And there is a module from TI used CSD18533Q5A for BLDC motor.
(www.ti.com/.../TIDM-LPBP-BLDCMOTORDRIVE;tisearch=Search-EN-Everything)
My question is what's the Continuous Drain Current of this MOSFET.
There are two information about Drain Current in the datasheet, one is in the table of "Absolute Maximum Ratings", it says 17A.
But in the other hand from "Figure 10. Maximum Safe Operating Area", if I use Vds=24V(DC), the max current is about 1A.
What's the different about these two information?
Thanks.
Have a nice day.
Golem