This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about ramp generator of LM5020-1

Guru 19655 points


Please let me know about ramp generator(below) of LM5020-1.

---------------------------------------------------------------

・I think that datasheet P8 write below contents, is it right?

 ⇒Slope ramp signal is compare with "(Error AMP output+1.4V)×1/3" by a PWM comparator.

・Ramp signal is 0V to 105mV(typ).

 In the case of Duty:50%, ramp signal is between 52.5mV to 105mV, is it right?

・If above is right, I think the 52.5mV is too small to Error AMP output.

 Is it mistaken where my way of thinking?

---------------------------------------------------------------

Best regards,

Satoshi

  • Hello Satoshi,

    (COMP - 1.4V) / 3 is one input to the LM5020-1's PWM comparator. The other input is the current sense signal plus the slope compensation signal, which at 50% duty cycle is an additional 52mV above the CS pin voltage (assuming no additional series resistance is added in series with the CS pin). You can reference this level back to COMP by multiplying by 3 and adding 1.4V.

    Regards,

    Tim