This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5000 compensation network

Guru 20090 points
Other Parts Discussed in Thread: LM5000

Hello,

I simluated LM5000 on webench with the following requirement.

Vin=26V~30V, Vout = 48C, Iout=0.5A, Ta=30deg.

As a result, phase margin is about 24.7° .
If I change the Rcomp from 20kohm to about 50kohm, phase maringe will be about 47°.
However, the Rcomp upper limit is 20kohm.

Could you please let me know this reason?

And since, I couldn't set the good compensation circuit on Webench, I  please let me know the reference compensation circuit value for above requirement.

Best Regards,
Ryuji Asaka