Dear Sirs
Please help review the following circuit about TPS2592AA.
I want set UV is 5V.
1.Is the R1 and R2 value right?
2.Is the pin BFET floating ok?
3.Is there any comment about the circuit?
Thanks
BRS
Nat
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sirs
Please help review the following circuit about TPS2592AA.
I want set UV is 5V.
1.Is the R1 and R2 value right?
2.Is the pin BFET floating ok?
3.Is there any comment about the circuit?
Thanks
BRS
Nat
Hello Wang,
I would suggest to go thru the TPS2592x design calculator to arrive the parts values.
This is very simple excel based tool.
This is available on below link,--
http://www.ti.com/product/TPS2592AA/toolssoftware
Regards
Dinehs