This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34z100 how to change parameters via uP after IT Enable (QEN is set)

Other Parts Discussed in Thread: BQ34Z100

Dear all,

I want to change parameters in ~200 pieces of BQ34z100, but QEN is set in each of them.

Is there another, easier way of changing parameters like "Design Capacity" than:

1. enter ROM mode via EVSoftware an then send *.senc file with update status = 0?

2. program *.gg file with correct parameters

I would like to use microcontroller instead EVSoftware. Becouse I can easily change software in it.

But to connect EVSoftware I need to solder wires to test pads on each board and some of them are coated with resin.

I can program gg file via uC so half of the solution is done. But I don't know how to program *.senc file to that IC

Is anyone know how to program *.senc file to BQ34z100 or know easier solution?

Best regards,

Damian.