I have an application that will consist of (mainly) a BQ24061, a lithium battery pack consisting of 2-4 18650 cells in parallel and a GMS modem. The intended design is to have the BQ charge the battery and the modem draw power off the battery. The GSM modem draws current in pulses of about 1.5 to 2.0 Amps. In the event that the modem is drawing power while the unit is connected to the charger, what will the BQ do? Its charge current is presently anticipated to be well below 1.0 Amps.