Can I depend on the PWRGD output to sink at least 400 uA current for the following operating conditions: input voltage VIN is less than 1.00V.
I ask, because on page 15 of the data sheet (SLV981C - JUNE 2010 - Revised August 2013) it states:
“The PWRGD is in a defined state once the VIN input voltage is greater than 1V but with reduced current sinking capability.”
which implies that PWRGD is undefined when VIN is 1V or less.
We have tested on our lab bench with operating condition VIN = 0V, and the PWRGD output is sinking current through pull down resistors - at least for a sample set of one TPS54521 IC. However, given the data sheet statement about VIN conditions where PWRGD is defined, I would like to get feedback from TI whether or not we can count on this in mass production, across all TPS54521 devices.