Hello,
I have just found a voltage regulator, LM2735, which could be a possible solution to my power supply (see the picture). But I am having hard time finding a proper transformer to the power supply, since there is nothing mentioned about the transformer in the datasheet (See the picture). My output voltage should be ±10VDC. The input voltage is +5VDC.
A transformer with a turn ratio of 1:5:5 should be good for this purpose, I think. But I am not sure which transformer type I should use (for example, audio & signal transformer, current transformer, power transformer....etc..).
It would be great if you also could suggest some names of manufacturer.
Thanks!
//OB