hi,
I have found a sample for TPS40210 and TPS6525. is it possible to get a sample with my requirement.
ex: TPS65251
output buck1 7.5V 3A
buck2 9V 2A
buck3 5V 2A
and for TPS40210 in sample nominal input voltage is 12V and output voltage is 25V. But, i have found a circuit in webench 12V to 100V 1A. So i want sample for 12V to 100V 1A.