Hi,
In an example battery protection circuit like in the image:
The protection used common-drain MOSFET pair at the low side. Is it because single MOSFET blocks only one direction current due to the body diode, so the common-drain pair is used?
In this circuit, does it make any difference if we use common-source connection for the same pair?
Extended:
We would like to use bq24616 to charge two 21V series. To completely isolate the two series, single MOSFET either at high or low end is not enough for the reasons above.
Could we use anti-direction MOSFET pairs to control which series to charge/discharge?
- Should common-source or common-drain be used?
- Should the pair be placed on the high side (bq→mosfet pair→battery→gnd) or the low side?
Hui