This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2678 Internal diode aProtection

Is there any internal diode for protection in case of a voltage at output without an input voltage??

  • There is a diode from the SW pin to the VIN pin.  However this is a parasitic and must not be allowed to turn on.

    So, to answer your question, No; there is no protection from a voltage on the output that is higher than the input.  An external Schottky diode can be used from Vout to Vin if desired.