This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217C LDO1 & LDO2 support how much current?

Hello Janice,

I am using TPS65217C along with AM335x Sitara Processor. I am interested on the specification of LDO2 maximum supported current? On sheet 1, 2 and 34 it is specified as max 100mA. On sheet 7 (Recommended operating conditions) it is mentioned as max 250mA.

Which specification is correct? Is there any special case in which it will only support 250mA.

Thanks & Regards,

Praveen Kajjam.