I have a PWM Buck DC-DC converter that runs fine with FETs like BSC27N04LSG or BSC039N06NS or Si7848bd. Recently TI introduced new superior FET, CSD18540Q5B, which offers lower Rds on, Lower Qcharge, Higher Current and voltage, etc. This transistor gets shorted immediately or in seconds when replace the other FETS mentioned above. The driver used is UCC27210 which can output max 4A (This one also get shorted when the FET get shorted too).
The PWM circuit runs fine and cool with other FETs, so I think I might missing something in its datasheet that makes it unable to work.
From datasheets, CSD18540Q5B, is an ideal replacement for the FETs mentioned above, but in practical it is not, why? ....What I am missing?