Hai,
does an LDO have internal circuit for sourcing more current Than that of what is provided at the input
regards
AGXIN
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Agxin,
LDO do not have that capability - Iout = Iin + Ignd, where Ignd is the current needed by the LDO for proper operation. A buck converter does have this capability as Pin = ~Pout (minus losses due to switching, the IC, etc.), so when it steps down the voltage it steps up the current.
Regards,
David
Hai sir
Thanks for your reply .In all LDO The component vendors are providing some feed back resistors are to be used in the output of the LDO to adjust the o/p voltage
are there any ways to limit the current of an LDO.( i.e the rated current is 3A can I fixed to 2A by some mechanism ?.or If I have to limit the current then I have to go
for an LDO with rated outputcurrent to be 2A ,How to fix eactly that this much rated current LDO will be sufficient for my application ?(i.e summing up all the load
currents powered byLDO is sufficient or any additional parameter is required to be included )what can I choose an ldo with a rated output current max when my
load current is known ? how much tolerance can I have from my Load current?.Thanks for responding again
thanks and regards
AGXIN,J