There is a problem of the test evaluation board BQ76940EVM I have a question.
BQ76940 Evaluation Software as a data variable and then set the value of the electronic load
When the load discharge the 10[A] works in normal operation
Questions:
When you run the BQSBB.EXE the data in BQ78350 BQ76940 in
Will be initialized.
To the electronic part 8 [A] over-discharge when the discharge FET OFF in the evaluation board BQ76940EVM
DATA MEMORY click, and open in BQSBB PF Status
Variable value in the AFE REGS are set to 0
Data variable values in the BQ76940 has changed with the wrong data.
I do not know why.
To receive the BQSBB user manual provided by TI's, Should I Buy?
(We are working to produce a 42V battery pack.) 10S2P
Test now trying to apply the newly released product from TI,
BACK-DATA are lacking too.
If you have gg.csv to provide a sample, please email us
Thank you.