This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27421-G1A shows 100% SOC before the charging completes

Hi all,

In my project  i am using bq27421-G1A Fuel Gauge for Li-Polymer Battery measurement.

I have configure fuel gauge battery parameters are:- 

Design Capacity = 108 mAh

Design Energy = 3.7 X 108 = 399.6 = Approx. 400 

TerminateVoltage = 3200 mV

TaperVoltage = 4200 mV

Taper Rate = 211    (I took taper current 5.11 ma so for that Taper Rate = Design Capacity / (0.1 * Taper Current))

All parameters updated successfully and it gives me proper current and voltage etc.

so my question is

1) For charging circuit i am using TI's BQ 24230  and in that charging current is set 50 ma and taper current set 5 ma (using appropriate resistor values).

So its work fine it charge battery at 51 ma and stop charging when charging current gradually decreases to  5 ma.

Now during charging, SOC (State of charge) increasing with drastic jumps at the end like 93 to 100 or 88 to 100 or 91 to 100.

 2 )  it shows me 100% SOC while   IC still charging my battery. 

Ideally If the taper rate is ( 0.1 * charge current)  for 5 ma taper current then Fuel gauge  should set its charging termination point accordingly.Means it shows me 100% when taper current reach around 5ma.

But in my case it shows 100% when even my charging current is not starts to decreases. So it is showing me full charging 100% early .

So Is there anything which i am missing or any update needed for proper measurement? 

How can i resolve these issues?