This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Accuracy of LM3409-Q1

Other Parts Discussed in Thread: LM3409-Q1, LM3409, LM3402

Dear all

My customer want to high accuracy LED driver. And I suggest  LM3409-Q1.

(Q1)Is it possible that  the solution within ±5% accuracy of  average LED current is designed using LM3409-Q1 ?  

(Q2)Please teach another IC or solution.

<spec>

Vin=12V (damp 36V)

I led=0.5A  (within ±5%  Ta=-40~105℃)

LED:2×1strings

Regards

Tomohiro Nagasawa