Hi,
Could you tell me about efficiency data in data sheet P6 Figure 1,2?
Please tell me the schematics and parts of when you get this efficiency vs Load Data?
Customer is worried about not able to get a good efficiency under the following conditions.
◇Vin=5.3V Vout=10V Iout=10-50mA L:NRG4026T100MN(10uH,85mΩ)
⇒10mA:η=78%、50mA:η=82%
Does the efficiency of the data sheet use the circuit of Page10 Figure7 (b) without isolation FET?
Best Regards,
Yusuke/Japan Disty