Hi
Our customer are going to reduce the softstart time. ( < 1ms )
For example, Css=1000pF, Tss= (Min)0.29ms (Typ)0.4ms (Max)0.51ms (@Css+/-30%)
Is it possible?
We understand the short time softstart will make the the inrush current to output cap.
However is there any limitation(min value) of that time for this device?
Could give us the recommended value(min) of that time if there are any concerned.
Regards,
Koji Hamamoto