Hi,
I'm looking at designing a bidirectional supply to run a thermoelectric cooler.
I've seen the DRV591, but it doesn't meet the requirements of my application.
My application requires currents of +/- 8 A with a voltage up to +/- 20 V to drive that current.
I'm thinking of using a PWM controller to run a voltage controlled buck converter where the feedback loop is closed around output current instead of output voltage.
Just wondering if TI has anything that might have already been done along these lines?
Thanks,
Ruz