Greetings.
I have the next problem:
I have the accumulator battery based on TS-LFP90AHA cells (LiFePO, 90 Ah, 2,5 - 4,2 V). This battery need for powered 600 W brushless motor. For battery mangment i take the controller BQ78PL114.
I was buy the BQ78PL114EVM-001 module for first experements.
And with this module I'm have some problems: when i'm powered small micromotor (current ~50-100 mA) - all ok
When i try to powered more powerfull motor (from airplane model brushless motor 350 W) at start battery controller gone to reset or hung.
At last time, bqWizard reported, what firmware was damaged and need to reflash firmware.
Please, advise me, what i can do for solve this problem?