This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

full bridge moseft driver

hi all, 

i'm designing a full bridge topology where the input voltage is 400V and an output voltage of 30V. i have some question about mosfet drivers:

1- is there any driver which can control the dead time and drive 4 outputs ( an output for each N-channel)? 

2- what is the best to use: tow drivers ( one for each tow mosfet), or one single driver for the 4 mosfets? 

3- do we have interest in controlling dead time since not all driver have this feature!! 

Thanks in advance!