This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help required for Identifying the Buck converter device for my requirement

Other Parts Discussed in Thread: TPS62510

Please find my design requirements below and help me to identify the part.

Design Requirement1:

Input Voltage – 3.3V(tolerance-9%)

Output Volatage – 1V(Tolerance -1%)

Output Current – 320mA

Device specification – Should have the “ENABLE & POWERGOOD” pins

 Design Requirement2:

Input Voltage – 3.3V(tolerance-9%)

Output Volatage – 1.2V(Tolerance -1%)

Output Current – 285mA

Device specification – Should have the “ENABLE & POWERGOOD” pins

 Thanks,

Jeyalakshmi