I have a BQ27500-V130 device. When I start the bqEasy wizard steb 1B "Load .DFI File" shows a warning message "The default .dfi file BQ27000V100_1_30.dfi was not found ..."
When I check the installation directory, the DFI file is missing, even though I installed what I think is the latest version of bqEasy (bqEV-EASY-HH SWSetup00.09.59_ bq27500v1.08_bq27500v1.20_v1.30_bqEASY v1.36). Can BQ27000V100_1_30.dfi (or BQ27500V100_1_30.dfi) be added to the installation or could someone send me a copy of the file?
Thanks,
James