This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55330 Vin 6.5V~8.4V Vout 8.5V,drop 4V at 3A load

Other Parts Discussed in Thread: TPS55330

Hi 
I test TPS55330 EVM board  Vin 6.5V~8.4V and  Vout 8.5V, that cause drop 4V at 3A load.
The current maybe only keep 10ms.

Is it correct design?

Please advice.

Thanks~

BR

Gary