This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about EV2300 and EV2400 of bq27621EVM

Guru 19645 points
Other Parts Discussed in Thread: EV2400

Please let me know about two point below of EV2300 and EV2400.

・Is EV2300/EV2400 needed to move bq27621EVM?

If EV2300/EV2400 isn't used, bq27621EVM can move an easy monitor, is it right?

・Customer using Windows7 32bit OS.

Which is most suitable for OS, EV2300 or EV2400?

(Windows XP:EV2300 , Windows 7 64bit:EV2400 , Windows 7 32bit:No information)

Best regards,

Satoshi

  • EV2400 is recommended for all versions of Windows.  It is the official solution for 64-bit Windows but also works fine with 32-bit Windows.

    The most significant hardware difference is that EV2400 has I2C pull-ups internally and EV2300 does not have internal I2C pullups.