This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61090 / About the value of L1.

Other Parts Discussed in Thread: TPS61090

Hi all.

The datasheet P14, P15 of TPS61090 shows the calculation of the L1 value.

●For example
・Vbat(Vin)=1.8V
・Vout=5V
・Iout=500mA
・ΔIL=IL*0.2

This datasheet shows that the value of L is 5.5uH.
Is this value correct?
I think the value is 6.6uH.

And could you tell me the value of the inductor L1 in the following case?
・Vin=1.8V
・Vout=5V
・Iout=0.4A

Best Regards,
Sho Ogane