First of all thank you for your help. I think I will choose the bq24292i, but I have some doubts that should be cleared up before. These are my questions:
1.-How can I power OFF my system if it is being powered from the battery? Maybe disconnecting BATFET, but then how can I power ON again?
2.- The USB PHY line that goes to the PSEL pin is VBUS?
3.- What is the difference between MAXIMUM INPUT CURRENT and FAST CHARGE CURRENT? I think that the first is the maximum current that should be draw from the power source and the second is the current that will charge the battery if enough current is available form the power source to feed the system and charge the battery, but I am not sure.
4.- In section "HIZ State with 100 mA USB Host" in the datasheet (page 21) states that if the power source is USB with 100 mA and the battery voltage is enough, the battery charger will enter high impedance mode and the system will be powered from the battery. These are my questions:
4.1- If there is no battery, the charger will not enter HIZ mode and will power the system?
4.2- If the battery voltage is ok and enter HIZ mode and meanwhile the battery is discharging to power the system, the charger will wake up and start to charge / feed the system when the voltage drops?
4.3- If I (with an I2C command) disable HIZ mode, the charger will start to charge the battery / feed the system?
5.- Say the maximum input current is set by the host via I2C to a certain value because I am using certain AC Wall Adapter. This limit is set everytime the entire system is powered on. Now if I change the Wall Adapter and is not capable to supply all the current, the charger will decrease the input current even below the maximum value to mantain the input voltage no matters how small the current should be?
Thank you in advance.