Hello,
I have selected BQ24295 for charging the battery. I have few questions.
1. What is the maximum current can be drawn from the PMID pin. The data sheet says IOTG_LSOCP LSFET cycle by cycle current limit 5A. This means that i can draw maximum of 5A from PMID pin.
2. Can we limit the current drawn from the PMID pin?
3. If I am drawing 2.5A from PMID pin and if I connect a external charger of 1A. What will be the behaviour of the IC.
Thanks & Regards,
Sreekanth