Hello,
For a new project, we have to design an isolated DC-DC power supply.
The minimum requirements for our project are:
Input: 9Vdc to 60Vdc
Output 1: 5Vdc ±5% @ 2A
Output 2: 24Vdc ±10% @ 0.2A
Topology: Flyback
If possible, without optocoupler for the feedback.
Could you please suggest an controller IC for the above requirements?
Thanks in advance.
Regards,
Filippo D. S.