This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lm22677 low temperature problem

Other Parts Discussed in Thread: LM22677

Hi,

I have problem with the Lm22677.

Attached you can find the circuit diagram.

The Vout  (C39) reaches 3.8V (rms) with a ripple of 300mV, instead of 3.4V

The rms value for the FB is over the datasheet range (1.45V) with a ripple of 300, instead of 1.304 (maximum data sheet value). mV.

I also tried to change and increase the C39 to 220uF, without a positive result.

Iout required is 3A