Hi All;
I'm working on a repair. The board has an LM2576T-5.0 simple switcher but instead of having the Feedback pin (4) connected directly to the Output (2), the board designer has a 5K6 resistor in between the pins.
I'm trying to find out what he is doing. I am assuming that he is using the feedback signal to provide somewhat more than the 5.0 volts output (the designer could have used the -ADJ version of the LM2576; I have no idea why it was decided not to) in order to trim the output voltage using some form of remote sensing, even though the 5K6 is soldered to the PCB.
My look thru datasheets, etc has not (yet) provided me with an answer, which is where I hope someone out in the Community can help.
What would the output be with 5K6 between the Feedback and Output pins?
I can't measure it, because the part is defective, with a near short (<100 ohms) between the in and out pins, and my customer is desperate to get the board going. My plan is, once I find out what the output would be, to use a -12V version or -ADJ version to get the board back to life, as it is 2 days delivery for the replacement -5 version.
Thanks!
Craig P. Renaud