Hello,
Could you please let me know transition output current of light load of TLV62090, TPS62085?
The customer would like to use TLV62090 or TPS62085 on the following conditions.
Vin=5V, Vout=1.1V, Iout=0.29A, Vout accuracy within 2%.
Since the these devices accuracy will be 3.7%(max) at the eco-mode, I would like to know the transition point.
Best Regards,
Ryuji Asaka